Force a Variable

At run-timeClosed In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running, all variables in the table widget are animated 1 with real-time values.

You can double-click on the value of a variable (or press the ENTER key when it is selected) to open a pop-up window that allows you to:

  • Unlock:
    Remove the lock on a variable so that it can be changed again by the runtime.